What do you need to know before getting your air conditioner installed?
Choose a high-quality heat pump system that will be reliable and long-lasting, with a high energy efficiency rating.
Make sure your home is well-insulated and the area around the indoor and outdoor units is clear. They need sufficient airflow to ensure the system works as efficiently as possible.
Air-to-air heat pumps get 80% of the energy they need to work from the outside air. Just 20% comes from electricity. Even so, you will need a consistent electricity supply to run the system.
Have your air conditioner installed professionally
Use a professional contractor to install your air conditioner.
Before starting, your heat pump installer will inspect your home to check what solution is best for your home.